This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP1G74: Hello, I want to use Power-on-switch as Tact SW (Low power module) as below

Part Number: SN74AUP1G74


 so draw Buffer(SN74AUP1G74) and D FLIPFLOP(SN74AUP1G74)

I wonder power-on maintained,  so confirm  this circuit is right.

Thank you, sir

  • Hello,

    I'm afraid your image did not make it through.

    To attach an image, start by selecting   at the bottom right of the reply box.

    Next use the   'Insert/Edit Media' button to attach your image. This requires that the image is stored as a file somewhere (not just on the clipboard).