For a new project of a 3.3v card inserted in the existing 5v system I have to choose drivers for the bus. The bus is passive of about 25cm in length. At the moment for the existing 5v cards, 74hct245 for bidirectional data bus and 74hct244 for unidirectional control line are used.
Which drivers are recommended as interface between new board at 3.3v and 5v system ?
I have see the 74lvcc3245 and 74lvc8t245 is the right choice ? The relative 244 do not exist ?
The driver can be 8 or 16 bits wide
Best regards
Enzo Bruno