This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74lvc573a: SN74LVC574ARGYR

Part Number: SN74LVC573A

Hello,

is the SN74LVC574ARGYR qualified for Ta -40°C to 125°C ?

On page 2 in the datasheet -40°C ..85°C is specified for VQFN20 package (this is the RGY type)

On abbendum page 2 the datasheet specifies -40°C to 125°C for the SN74LVC574ARGYR.

What is correct? what parameters in this datasheet are valid for the SN74LVC574ARGYR?

thanks

Ronny