This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD74HC123: tW = 0.45 Rx Cx in case of Vcc = 3.3V and Ψjt

Part Number: CD74HC123


Hi all

Would you mind if we ask CD74HC123?

<Question1>
There is the formula "tW = 0.45 Rx Cx  in case of  Vcc = 5.0V" on the datasheet.
In case of Vcc=3.3V, is tW's caluculation a the same as  tW = 0.45 Rx Cx?
Compared with using calculation "tW = 0.45 Rx Cx", the result of measurement was 1.5 times. 
How much will be the tolerance?

<Question2>
And then, how much is Ψjt?

Kind regards,

Hirotaka Matsumoto

  • Hi Matsumoto-san,

    <Question 1>

    The calculation of the pulse width is done by the equation tW = k*Rx*Cx. For the 5.0V case the value of k is .45.

    To find the value for the other voltages, the following table provided in the datasheet can be used.

    Also please make sure that the values of Cx and Rx are chosen correctly. Here is a table also found in the datasheet that helps with finding these values.

    <Question 2>

    To find Ψjt for you, I will need the full part number. If you are looking for CD74HC123M96 for example the Ψjt = 10.1 C/W however this value will differ for each package.

    Thank You!

    - Karan

  • Karan san


    Thank you so much for your reply.

    <Question 2>
    To find Ψjt for you, I will need the full part number. If you are looking for CD74HC123M96 for example the Ψjt = 10.1 C/W however this value will differ for each package.
    ->CD74HC123PWR. We need the information with PWR package.

    Kind regards,

    Hirotaka Matsumoto

  • Matsumoto san,

    I have submitted the thermals request for the PWR package. Please allow up to a week to get this value for you.
    I am sorry for this delay.

    Thanks!
    - Karan
  • Karan san

    Thank you so much for your support.

    Ok, we are waiting for your update.

    Kind regards,

    Hirotaka Matsumoto

  • Karan san

    Thank you so much for your CD74HC123's support always!

    In addition to PWR's Ψjt, we have additional questions about tW.

    <Customer's circumstance>
    Our customer would like to set tW=100 to 200ms.
    With considering K=0.48, compared with measurement result, calculation value is smaller than measurement result as follows;
    -Calculation value : 124ms
    -Measurement result : 173ms

    The customer caluclated the value as follows;
    Ta=25C
    Cx=0.953uF(3.3V, it contains Cbias, without non-DCbias=2.2uF)
    Rx=270kΩ
    tW = 0.48 * 0.953uF * 270kΩ = 124ms
    If there are some tolerance like as temparature, resistor, and capcitance, we assume that max value will be 160ms.
    So, what is cause of the difference between calculation value and customer's measurement result?
    If you have some advice, could you let us know?

    Kind regards,

    Hirotaka Matsumoto

  • Hello Matsumoto-san,
    The datasheet table for K factor is only listed for 10nF. This value will typically decrease with larger capacitors, and increase with smaller capacitors.

    This is one reason why we always recommend prototyping the circuit prior to production.

    From the information you have provided, your capacitor produces a K value of:
    0.173 = K * 0.953uF * 270 kΩ
    K = 0.672

    You can expect that the K value will remain consistent with similar size/style capacitors.

    We expect up to see up to 10% variation across temperature/process for pulse width from a monostable multivibrator (typically under 1%, not including manufacturing and temperature variation in the timing components), so I would recommend getting as close to 150ms as possible to guarantee that the pulse will always fall in the desired range:

    0.150 = 0.672 * 0.953uF * R
    R ~= 234 kΩ

  • Emrys san

    Thank you for your reply!
    OK, we got it.

    And we are waiting for Ψjt value with PWR package.

    Kind regards,

    Hirotaka Matsumoto


  • Hello Matsumoto-san,

    For the PWR package Ψjt = 3.5 C/W.

    Thanks!
    - Karan