This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74ABT827: sn74abt827

Part Number: SN74ABT827

I would like to know if having a pullup on the output of the SN74ABT827 creates any issues with the specifications.

The VCC is +5V and the pullup is 10K to VCC.

Normally Cmos outputs do not like to have pullup or down resistors.

This part does not have a high side output diode to the VCC rail. It only has a low side diode to GND.

Hence the caveat is in the specifications and  it appears that adding a pullup to VCC can potentially inject current into the output pin which generally is not accepted without high side diode.

Are there issue with this pullup on the output?