Other Parts Discussed in Thread: TXS0206A
Dear Experts,
I have an issue with TXB0104 used to translate 5V <-> 3.3V to connect an MCU ATMEGA1284P to a SD-card. Please see attache part of schematic.
After power up the TXB0104 often do not work. I control the OE using a small transistor to switch to HIGH ( 3.3V ) 500ms after Power is up which seemed long enought to get a stable VCCA and VCCB. I think it should be possible to drive OE directly by 5V logic of MCU because the OE input is 5V tolerance but I´m not sure. The OE is pulled down by 3.9K resistor. The SPI interface is initialized before OE is set to HIGH
The question is why TXB0104 often do not work after power up ??
Thanks a lot for all your input.
Best Regards
Karsten