Hi Guys
Customer is using our SN74LVC2G86. There is a detailed question about the input logic voltage level:
There are two understandings of Vih in the SN74LVC2G86 SPEC:
1. The minimum Vih value is 2V, assuming Vih is 2.1V, indicating that the input voltage is greater than 2V, the logic is H; when the input voltage is 2.0V, it is less than Voh, then the logic is L; If the input voltage is 1.9V, the judgment logic is L because it must be less than the Vih value;
2. If the input voltage is greater than or equal to 2V, it is judged as H; in order to meet the requirements of the actual chip, it is possible to judge the logic to be H at 1.9V or 1.95V or 1.98V;
So Which one is correct? Or what is the correct way to understand the Vih of the logic voltage?
Thank you~
Thanks
-Pengfei