This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4541B-MIL: shorter count value than expected

Part Number: CD4541B-MIL

Hello,

I am actually designing a CD4541 to allow it to count at 9.5 s approximativly

I have done several tests with Rtc and Ctc couples but none of them gave me a correct value. Each test i've made gave me a time shorter than expected.

For example, i have settle a count value of 8192, a Rtc of 105 kOhm and a Ctc of 4.7nF. I am expecting a time value between 9.11s and 9.48 s but it gave me 8.76s on the five samples i've built.

And the same thing happened with each couple i used.

Is the formula in the datasheet correct ? the 2.3 factor is the most precise one or has it been shortened to be more "readable" ?

Please let me know .

Best regards