Part Number: CD4541B-MIL
Hello,
I am actually designing a CD4541 to allow it to count at 9.5 s approximativly
I have done several tests with Rtc and Ctc couples but none of them gave me a correct value. Each test i've made gave me a time shorter than expected.
For example, i have settle a count value of 8192, a Rtc of 105 kOhm and a Ctc of 4.7nF. I am expecting a time value between 9.11s and 9.48 s but it gave me 8.76s on the five samples i've built.
And the same thing happened with each couple i used.
Is the formula in the datasheet correct ? the 2.3 factor is the most precise one or has it been shortened to be more "readable" ?
Please let me know .
Best regards