Hi,
I also wanted to know the input voltage threshold (Vt+, Vt-) limit variation with respect to voltage and temperature. Looks like, the excel link in another thread pointed here, provided only the variation w.r.t. 3.3V input variation. could you please help me with the temperature range of 0 to 75 degC Ambient and input voltage 5V with 5% variation.
Thanks in advance for your help!
Thanks & Regards
Muthu A