This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
Customer has a need to convert a signal whose high-level range is between 2.4V-5V to the standard 3.3V / 1.8V LVCMOS level.
Can LSF0102 support this? Thanks.
Hi,
SN74LVC2T45 only have 0.7*VDD high level when it is 5VDD power supply. Can it support 2.4V when 5V supply?