This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC162244A: 26 ohms series resistors in IBIS model?

Part Number: SN74LVC162244A

The SN74LVC162244A datasheet states that ‘Output ports have equivalent 26 ohms series resistors, so no external resistors are required’. I’m using the sn74lvc162244a.ibs IBIS model (rev 1.1 - dated 12-17-2004) and getting 600mV undershoot with no series, passes when adding a 33 ohm series by the driver.

Do the sn74lvc162244a.ibs output models include the 26 ohm series?