This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AXC4T774-Q1: Can I use SN74AXC4T774-Q1 for general GPIO LEVEL conversion?

Part Number: SN74AXC4T774-Q1


I am using the LS1012A,

which is a 1.8V processor, and I want to connect the external interface to 3.3V.

So, I want to use SN74AXC4T774-Q1, but there is no GPIO in the application of TI homepage.

Can I use GPIO?