This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2244A: SN74LVC2244A fanout capability

Part Number: SN74LVC2244A


Dear  expert,

I have a quaestion about SN74LVC2244A.

I want to use this chip to fanout signal from 1 input  to 20 outpout to another board by short FPC cable(10cm)  to FPGA convert card.

the signal rate is less than 1M.

there are 6 kid of signals totally also to fanout from 1 input to 20 output.

in orde to layout easily, I perfer to use  SN74LVC2244A (VCC=2.5V).

I read the datatsheet of it , but I didn't  see input current related spec: Input current low max spec & Input current high max spec

I want to use IOH/IIH  , IOL/IIL to calculate the fanout  ability.

Thanks a lot!

Alex 

13011010317

guowang.li@quantum-qtm.com