Other Parts Discussed in Thread: TXB0104, LSF0204, LSF0108, SN74CBT3384A, TXS0104E
I need to use the TXB0304 in a 5-3.3V application.
Max operating voltage is listed a 3.6V
How does the higher voltage affect operation and reliability?
End product is use in office environment. ~22c.
I've tried the TXB0104 but in the application it only drives the B side (+5) to 2V because of termination on customers CPU card.
The TXB0304 drives it to 4.3V.... and their application works.
Thanks.