This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVCC3245A: possibility of damage VCCA:3.3V and VCCB:0V

Part Number: SN74LVCC3245A

Dear Specialists,

My customer is considering SN74LVCC3245A and have a question.

I would be grateful if you could advise.

---

We are considering whether we can supply only 3.3V to update the F/W of 3.3V microcontrollers.

Because it is not necessary to operate the SN74LVCC3245A when writing to F/W.

When VCCA: 3.3V, VCCB: 0V, is there a possibility of damage?

A1-8, DIR may be applied with 3.3V.
G # is fixed 3.3V (inactive).

Is it possible to use under these conditions?

---

I appreciate your great help in advance.

Best regards,

Shinichi