Part Number: RM46L852
I put my Processor into sleep_mode.
And I want to wakeup mcu using DCAN1.
However it doesn't work.
How to wakeup process from CAN message?
My test code is like below.
void mcusleep(void)
{
canREG1->CTL |= (((uint32_t) 1U << 2 ) /* Enable Status Interrupts*/
| (uint32_t)((uint32_t)0x1U << 25U));
canREG1->ES |= ((uint32_t)0x1 << 9);
canREG1->CTL &= ~(uint32)(0x00000041U);/*Clear Init Bit*/
pcrREG->PSPWRDWNSET1 &= ~(uint32)(0x00000003U); /*Power Down DCAN1*/
vimREG->WAKEMASKSET0 =0xFFFFFFFF;
vimREG->WAKEMASKSET1 =0xFFFFFFFF;
vimREG->WAKEMASKSET2 = 0xFFFFFFFF;
vimREG->WAKEMASKSET3 = 0xFFFFFFFF;
vimREG->WAKEMASKCLR0 = 0xFFFFFFFF;
vimREG->WAKEMASKCLR1 = 0xFFFFFFFF;
vimREG->WAKEMASKSET0 = 1U << 16U | 1U << 29U;
_enable_IRQ();
/** Setup Flash Banck Access Control **/
//flashWREG->FBAC = (0x0F << 8) | (0x0F);
flashWREG->FBAC = 0x00000000U
|(uint32)((uint32)15U<< 8U) //BAGP
|(uint32)((uint32)15U); //VREADST
/** - Setup flash bank power modes */
flashWREG->FBFALLBACK = 0x00000000U
| (uint32)((uint32)SYS_SLEEP << 14U) /* BANK 7 */
| (uint32)((uint32)SYS_SLEEP << 2U) /* BANK 1 */
| (uint32)((uint32)SYS_SLEEP << 0U); /* BANK 0 */
// Flash pump - all pump circuits disabled
flashWREG->FPAC1 = flashWREG->FPAC1 & ~(0x1U);
flashWREG->FPAC2 = 0x0;
/** - Setup GCLK, HCLK and VCLK clock source for normal operation, power down mode and after wakeup */
systemREG1->GHVSRC = (uint32)((uint32)SYS_LPO_HIGH << 24U)
| (uint32)((uint32)SYS_LPO_HIGH << 16U)
| (uint32)((uint32)SYS_PLL1 << 0U);
/** - Setup asynchronous peripheral clock sources for AVCLK1 and AVCLK2 */
systemREG1->VCLKASRC = (uint32)((uint32)SYS_LPO_HIGH << 8U)
| (uint32)((uint32)SYS_LPO_HIGH << 0U);
sleep_clk = (uint32)((uint32)1U << 0U)
|(uint32)((uint32)0U << 1U)
|(uint32)((uint32)1U << 3U)
|(uint32)((uint32)1U << 4U)
|(uint32)((uint32)0U << 5U)
|(uint32)((uint32)1U << 6U)
|(uint32)((uint32)1U << 7U);
systemREG1->CSDIS = sleep_clk;
while((systemREG1->CSDIS & sleep_clk) != sleep_clk)
{
/* Wait */
}
systemREG1->CDDIS = 0x1 //RTICLK is enabled for wakeup
| (uint32)((uint32)1U << 0U ) /* GCLKOFF */
| (uint32)((uint32)0U << 1U ) /* HCLK OFF */
| (uint32)((uint32)0U << 2U ) /* VCLKP OFF */
| (uint32)((uint32)1U << 3U ) /* VCLK2 OFF */
| (uint32)((uint32)0U << 4U ) /* AVCLK 1 OFF */
| (uint32)((uint32)1U << 5U ) /* AVCLK 2 OFF */
| (uint32)((uint32)1U << 8U ) /* VCLK3 OFF */
| (uint32)((uint32)1U << 9U ) /* VCLK4 OFF */
| (uint32)((uint32)1U << 10U) /* AVCLK 3 OFF */
| (uint32)((uint32)1U << 11U); /* AVCLK 4 OFF */
asm( " NOP");
asm( " NOP");
asm( " NOP");
asm( " WFI");
asm( " NOP");
asm( " NOP");
asm( " NOP");
}