Part Number: MSP432E401Y
Actual part number is MSP432P401R, wasn't able to find it in the part number field. My project uses an LCD screen to display messages to an operator for their input. When the device is turned on there's a startup screen during which everything is initialized and the screen is meant to transition through a timer interrupt. Two times out of roughly eighty power cycles, the startup screen gets stuck and never transitions to the main menu. The device was reflashed with some additional code that is meant to do a marginal read of the flash on startup, we've run 50 more times with that code and haven't seen this issue again.
Is this an issue with the Interrupt Vector Table being corrupted somehow on startup? What would you recommend us to check?
Thanks,
David