Other Parts Discussed in Thread: TM4C1294NCPDT
Hi,
I use the MSP-EXP432P401R development kit, and using the TM4C1294NCPDT burner I burn to the MSP432P401R on another PCBA.
The first time I loaded the program (for that matter I used the example pwmled2_MSP_EXP432P401R_nortos_ccs), through the debugger, the program loaded. Through the FLASH button it did not work.
The second time I loaded the program (same program), I got this error:
CS_DAP_0: Error connecting to the target: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 9.5.0.00143)
It repeated itself several times in exactly the same way.
I updated all the software, and all the firmware I could.
Anyone have an idea what could be causing the error?