Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: CODECOMPOSER
At my company we used in the past th CodeComposer 7 environment and we did not use "boot_emac_flash" or any other sw. we just had the project we developed and we used the far away programing LM flasher service.
Today, using CC (code composer) version 10 I am using the "boot_emac_flash" as something basic to burn to work with and then my project itself that is burned (at address 0x4000).
1 - What is the diference between the 2 bootloader ways?
when I want to upgrade from ver 7 to ver 10 it cannot be done.
I have systems with over a hundred boards each , with version 7 CC and I need to update it to version 10 with the new code version, that can't be done, only via serial service.
2 - Is there a way to have this LM flasher service using CC 10 version without needing "boot_emac_flash" ?
3 - If (2) isnt posible, how can I upgrade the CC 7 version project to my new CC 10 version code using the LM flasher (for my over 100 boards systems).