Part Number: MCU-PLUS-SDK-AM243X
Dear Community,
we are currently evaluating the latest release of the MCU-PLUS-SDK-AM243X with focus on the ProfiNet demo for the launchpad.
We managed to run the demo on the launchpad and add the device to ProfINet network with a Siemens S7 as ProfiNet Master.
As we have several questions, is there further documentation for the API and the Industrial Ethernet stacks available?
The collection of our questions:
- Cyclic Data:
- How is the cyclic data mapped from the application side via the stack API to the PLC side (represented by the GSD file)?
- How to check for data written by the PLC to the device (Output Data)? Is there a manual how to do this?
- How are the three buffers required by the input and output buffer function handled and what are the restrictions here (PN_API_DEV_setOutputDataBuffer, PN_API_DEV_setInputDataBuffer)?
In the demo the same buffer is provided for three buffer parameters required by the functions.
- Acyclic Data
- Is there a demo how to handle acyclic data and how the data is structured for this?
- Evaluation License
- We faced the issue, that the demo stops to work after some time (about 1h)
- Is there a possibility to get a demo without time limitations?
- To our understanding, the license for the Industrial Ethernet Stack is provided by the MCU itself.

- We faced the issue, that the demo stops to work after some time (about 1h)
Thanks in advance for you help (and sorry for asking so many questions ;) )
BR
Robin