Part Number: AM2634
Other Parts Discussed in Thread: UNIFLASH
Hi all
We try to uniflash by UART0 on our customer board with SDK V8.2
AM263x MCU+ SDK: Flashing Tools (ti.com)
We can Downloading *.appimage (210772byte) successfully by python uart_uniflash.py,
>python uart_uniflash.py -p COM28 --cfg=default_sbl_qspi.cfg Parsing config file ... Parsing config file ... SUCCESS. Found 3 command(s) !!! Executing command 1 of 3 ... Found flash writer ... sending sbl_prebuilt/am263x-cc/sbl_uart_uniflash.release.tiimage Sent flashwriter sbl_prebuilt/am263x-cc/sbl_uart_uniflash.release.tiimage of size 49534 bytes in 7.06s. Executing command 2 of 3 ... Command arguments : --file=../../am263x_zcu_sbl/Debug/am263x_zcu_sbl.tiimage --operation=flash --flash-offset=0x0 Sent ../../am263x_zcu_sbl/Debug/am263x_zcu_sbl.tiimage of size 124942 bytes in 15.17s. [STATUS] SUCCESS !!! Executing command 3 of 3 ... Command arguments : --file=../../am263x_zcu/Release/am263x_zcu.appimage --operation=flash --flash-offset=0x80000 Sent ../../am263x_zcu/Release/am263x_zcu.appimage of size 210772 bytes in 22.64s. [STATUS] SUCCESS !!! All commands from config file are executed !!!
We can't completed downloading *.appimage (756319byte) by python uart_uniflash.py,
C:\GIT_HH\TI_AM263x_new\evw\tools\boot>python uart_uniflash.py -p COM28 --cfg=C:\GIT_HH\TI_AM263x_new\evw\tools\boot\sbl_prebuilt\am263x-cc\default_sbl_qspi_zcu.cfg
Parsing config file ...
Parsing config file ... SUCCESS. Found 3 command(s) !!!
Executing command 1 of 3 ...
Found flash writer ... sending sbl_prebuilt/am263x-cc/sbl_uart_uniflash.release.tiimage
Sent flashwriter sbl_prebuilt/am263x-cc/sbl_uart_uniflash.release.tiimage of size 49534 bytes in 7.69s.
Executing command 2 of 3 ...
Command arguments : --file=sbl_prebuilt/am263x-cc/sbl_qspi.release.tiimage --operation=flash --flash-offset=0x0
Sent sbl_prebuilt/am263x-cc/sbl_qspi.release.tiimage of size 56206 bytes in 8.65s.
[STATUS] SUCCESS !!!
Executing command 3 of 3 ...
Command arguments : --file=../../am263x_zcu/Release/am263x_zcu.appimage --operation=flash --flash-offset=0x80000
Sending ../../am263x_zcu/Release/am263x_zcu.appimage: 756317bytes [01:13, 10725.90bytes/s]recv error: getc timeout in start sequence
Sending ../../am263x_zcu/Release/am263x_zcu.appimage: 756319bytes [01:25, 10725.90bytes/s]expected sequence 2, got (seq1=1, seq2=1), receiving next block, will NAK.
recv error: purge, requesting retransmission (NAK)
Sending ../../am263x_zcu/Release/am263x_zcu.appimage: 756319bytes [01:30, 10725.90bytes/s]
[ERROR] XMODEM recv failed, no response OR incorrect response from EVM OR cancelled by user,
Power cycle EVM and run this script again !!!
BR
JAY