Part Number: AM2432
I need to connect PHY chip (LAN8740A-EN) using MII interface to AM2432 but I am not sure if I am using right balls on AM2432.
I think that I have following two options to connect AM2432 to the PHY chip:
OPTION 1
| BALL | SIGNAL | PHY CHIP PIN |
| Y6 | MIO0_MDC | 16 (MDIO) |
| AA6 | MDIO0_MDIO | 17 (MDC) |
| Y7 | MII0_RXD0 | 11 (RXD0/MODE0) |
| U8 | MII0_RXD1 | 10 (RXD1/MODE1) |
| W8 | MII0_RXD2 | 9 (RXD2/NPME/RMIISEL) |
| V8 | MII0_RXD3 | 8 (RXD3/PHYAD2) |
| Y8 | MII0_RXDV | 26 (RXDV) |
| V13 | MII0_RXER | 13 (RXER/RXD4/PHYAD0) |
| AA7 | MII_MR0_CLK | 7 (RXCLK/PHYAD1) |
| AA8 | MII0_TXD0 | 22 (TXD0) |
| U9 | MII0_TXD1 | 23 (TXD1) |
| W9 | MII0_TXD2 | 24 (TXD2) |
| AA9 | MII0_TXD3 | 25 (TXD3) |
| Y9 | MII0_TXEN | 21 (TXEN) |
| V9 | MII_MT0_CLK | 20 (TXCLK) |
OPTION 2
| BALL | SIGNAL | PHY CHIP PIN |
| Y6 | MIO0_MDC | 16 (MDIO) |
| AA6 | MDIO0_MDIO | 17 (MDC) |
| W11 | MII1_RXD0 | 11 (RXD0/MODE0) |
| V11 | MII1_RXD1 | 10 (RXD1/MODE1) |
| AA12 | MII1_RXD2 | 9 (RXD2/NPME/RMIISEL) |
| Y12 | MII1_RXD3 | 8 (RXD3/PHYAD2) |
| W12 | MII1_RXDV | 26 (RXDV) |
| AA13 | MII1_RXER | 13 (RXER/RXD4/PHYAD0) |
| U11 | MII_MR1_CLK | 7 (RXCLK/PHYAD1) |
| AA10 | MII1_TXD0 | 22 (TXD0) |
| V10 | MII1_TXD1 | 23 (TXD1) |
| U10 | MII1_TXD2 | 24 (TXD2) |
| AA11 | MII1_TXD3 | 25 (TXD3) |
| Y11 | MII1_TXEN | 21 (TXEN) |
| Y10 | MII_MT1_CLK | 20 (TXCLK) |
I need to know if the above selections are correct. In addition I was not able to figure out how to connect the CRS and COL signals. These are pin 14 (CRS) and pin 15 (COL/CRS_DV/MODE2) on the LAN8740A-EN Ethernet PHY chip we intend to use. Can you let me know which balls on AM2432 to use for those two signals.