This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1230E6PM: TM4C1230E6PM

Part Number: TM4C1230E6PM

Hi,

I am using TM4C1230E6PM microcontroller, I want to save unsigned long number (4 Byte) information in memory, when power goes its will save this variable data in memory and when its Power ON, can retain this 4 byte value.

What is the best way and where to its memorize this data on chip memory

As per data sheet 3 option, Kindly confirm which is most suitable for 4 Byte Data

■ 32 KB single-cycle SRAM
■ 128 KB Flash memory
■ 2KB EEPROM

also share C code for the READ and WRITE operation for this ON chip memory

Thanks in Advance