This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am using the TMS570LC4357 and I have a question about the initial configuration value for one of the system registers, Peripheral Asynchronous Clock Configuration 1 Register (VCLKACON1).
In HL_system.c the function systemGetConfigValue() returns either initial or current value for each register.
For the initial value of VCLKACON1 systemGetConfigValue() returns SYS2_VCLKACON1_CONFIGVALUE.
SYS2_VCLKACON1_CONFIGVALUE is defined in HL_system.c as follows
#define SYS2_VCLKACON1_CONFIGVALUE ( (uint32)((uint32)1U << 24U) \
| (uint32)((uint32)1U << 20U) \
| (uint32)((uint32)SYS_VCLK << 16U)\
| (uint32)((uint32)1U << 8U)\
| (uint32)((uint32)1U << 4U) \
| (uint32)((uint32)SYS_VCLK << 0U) )
However, in mapClocks() the initial value of VCLKACON1 is
systemREG2->VCLKACON1 = (uint32)((uint32)(1U - 1U) << 24U)
| (uint32)((uint32)0U << 20U)
| (uint32)((uint32)SYS_VCLK << 16U)
| (uint32)((uint32)(1U - 1U) << 8U)
| (uint32)((uint32)0U << 4U)
| (uint32)((uint32)SYS_VCLK << 0U);
i.e. the two values are different
Can you confirm that SYS2_VCLKACON1_CONFIGVALUE is wrong and that the initialisation in mapClocks() is correct?
Thank you.
Hi Andrew,
I discussed with my internal team and i got confirmation that it is a HALCoGen Bug and initial value return by systemGetConfigValue function should need to be correct. Thanks for let us know this bug and we will fix this in next version of HALCoGen.
--
Thanks & Regards,
Jagadish.