Part Number: AM2634
I am trying to find the handling of the MCAN register MCAN0_CFG_TXBRP.
From the Datasheet, TRM & Advance TRM its not clear when the TRP bits will be cleared, as these are read only registers, so this must be cleared automatically.
I am using the Tx buffers instead of TxFIFO.I believe the respective bit(0-31) indicates which Tx buffer has a pending message that is yet to transmit on the CanBus.
it will be helpful to know the the sequence need to be followed to process multiple Tx messages using TxBuffer.