Part Number: TMS570LC4357
Hi experts,
When implementing the ECC-faultinjection test CAN15 mentioned in the Safety Manual, we encountered the following Problem.
After initializing the CAN-RAM with ECC-Enabled. we flip one bit and then read from the adress where we flipped the bit.
When checking ESM and ECCDIAG STAT we noticed that single bit error as well as double bit error flags get set. (e.g. for CAN1 ESM 1.73 and 1.21)
The result is similar with CAN2, 3 and 4.
(Q1) Is this the expected behaviour?
Thank you and best regards,
Max