Other Parts Discussed in Thread: AM4378
I am goal is to connect JTAG to AM437x-GP EVM to Read some register values.
Here is the steps i fallowed:
1. installed latest CSS software on windows. i.e CCS12.1.0.00007_win64
2. installed ti emulator package from XDS110 website i.e ti_emupack_setup_9.2.0.00002_win_64.
3. Created a Debug Target Configuration file i.e NewTargetConfiguration.ccxml with Connection as TI XDS110 USB Debug probe.
Board or Device type as AM4378
4. I updated XDS110 probe firmware also to latest version.
>xdsdfu.exe -e
USB Device Firmware Upgrade Utility
Copyright (c) 2008-2019 Texas Instruments Incorporated. All rights reserved.
Scanning USB buses for supported XDS110 devices...
<<<< Device 0 >>>>
VID: 0x0451 PID: 0xbef3
Device Name: XDS110 Probe with CMSIS-DAP
Version: 3.0.0.13
Manufacturer: Texas Instruments
Serial Num: 00000000
Mode: Runtime
Configuration: Standard
Found 1 device.
When i click TestConnection button. i am getting below error.
[Start: Texas Instruments XDS110 USB Debug Probe_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\NALLAM~1\AppData\Local\TEXASI~1\
CCS\ccs1210\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'May 7 2020'.
The library build time was '21:10:18'.
The library package version is '9.2.0.00002'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-266' (0xfffffef6).
The title is 'SC_ERR_XDS110_CPLD_UPDATE'.
The explanation is:
An internal error occurred. The CPLD image update failed. Unplug and
re-plug the XDS110, and try again.
[End: Texas Instruments XDS110 USB Debug Probe_0]