Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
Hello,
I am trying to use the example to send a CAN frame on early samples
I have SDK 0.58 and CSS 12.0.0, working fine with the early samples
I alredady succeded to send CAN messages with the exact same HW and CSS12.3 (not for early samples)
HW is correct, oscillator correctly configured, I think I put the correct configuration in syscfg file but no frames are emitted, bus is idle
Microcontroler is awake and oscillators correct, I have a GPIO set as a n output toggeling from a timer at 2ms, that works well, it's divided to send a frame every 100ms
Is there a guide regarding the setting of CAN in syscfg? I try to send a 8 bytes frames in CAN HS 500kbit/s
Please find bellow the related config I have now - thanks
Thanks