This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: CAN tx example on early samples

Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG

Hello,

I am trying to use the example to send a CAN frame on early samples

I have SDK 0.58 and CSS 12.0.0, working fine with the early samples

I alredady succeded to send CAN messages with the exact same HW and CSS12.3 (not for early samples)

HW is correct, oscillator correctly configured, I think I put the correct configuration in syscfg file but no frames are emitted, bus is idle

Microcontroler is awake and oscillators correct, I have a GPIO set as a n output toggeling from a timer at 2ms, that works well, it's divided to send a frame every 100ms

Is there a guide regarding the setting of CAN in syscfg? I try to send a 8 bytes frames in CAN HS 500kbit/s

Please find bellow the related config I have now - thanks

Thanks