Other Parts Discussed in Thread: LP5890, TLC6983
Hi,
When using SSI1 as a master with the mode as either SSI_FRF_MOTO_MODE_1 or SSI_FRF_MOTO_MODE_3 I see a glitch to 0V on the serial out pin at the very end of the frame, just as FSS returns high. I do not see any glitch when using SSI_FRF_TI (TI continuous mode). I am using a 10K resistor as the pull up for the serial out pin. The pin configurations are those for SSI1 from the TI PinMux tool with no further modifications.
Is this due to me doing something wrong please?
Thanks,
Matthew