This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello,i install the SDK4.4.1 and want to bulid the am273x demo,first i set to the mmWave Build Environment Configured and then cd to the path "ti\mmwave_mcuplus_sdk_04_04_00_01\mmwave_mcuplus_sdk_04_04_00_01\ti\demo\am273x\mmw",i use the “gmake all”to build the demo,but get the error in cmd “No rule to make target 'obj_am273x/mmwdemo_adcconfig.oer5f', needed by 'mssDemo'. Stop.”,i hope somebody can tell me how to build the am273x demo in correct。the error figure is as following:
Hi,
Here I have tried to build the same demo and you can see the build is successful.
So, I'll suggest you to follow the below steps
- Set MMWAVE_SDK_DEVICE=am273x in setenv.bat file(in mmwave_mcuplus_sdk_04_04_00_01/scripts/windows folder) and save it
- Open command prompt, change directory to mmwave_mcuplus_sdk_04_04_00_01/scripts/windows folder
- Run setenv.bat in the prompt
- In the same prompt change the directory to mmwave_mcuplus_sdk_04_04_00_01/ti/demo/am273x/mmw folder
- Run gmake clean
- Run gmake all
Please follow those steps and specially gmake clean.
Regards,
Anirban