Part Number: TM4C129XNCZAD
Hello,
The system that I am working on has a web server hosted on the TM4C129XNCZAD microcontroller. The client sends periodic HTTP requests to the server each 5 seconds. Sometimes the TM4C board crashes and I want to get to the root cause.
I investigated the crash info and it led me that it happens in the following API from the NDK stack: SockPcbFind ,
Specifically at the following condition:
/* Local port NULL means socket is not bound */
if( !ps->LPort )
continue;
I assume that the rate at which the client sends its requests to the server might be fast (every 5 seconds), Is that a possible reason for the crash?
Here is the crash info:
======================================== Crash Report ==============================================
Error ID : 0x11450000
Error Message: E_busFault: PRECISERR: Immediate Bus Fault, exact addr known, address: f0500090
Error Arg0 : 0xab008
Error Arg1 : 0xf0500090
file Name : UNKOWN
Line Number : 1172
Module Number: 32814
End Dump Error info
End Error Hook
Start Exception
======================================== Crash cause info Details: ==============================================Bogus Exception return value: 0x000b6bab.
Hard Fault ID = 0x11170000 - Details: FORCED
Exception occurred in ThreadType_Task.
Task name: User's NDK Stack Thread, handle: 0x2003e3e4.
Task stack base: 0x200313d0.
Task stack size: 0x800.
R0 = 0x00000000 R8 = 0xb600010a
R1 = 0x4400010a R9 = 0x00000000
R2 = 0x00005000 R10 = 0x200319d8
R3 = 0xf0012140 R11 = 0x00005000
R4 = 0xf04ffffc R12 = 0xcb3aa600
R5 = 0x000024ea SP(R13) = 0x200319a0
R6 = 0x00000009 LR(R14) = 0x000b6bab
R7 = 0x4400010a PC(R15) = 0x000c8324
PSR = 0xa1000000
ICSR = 0x00423803
MMFSR = 0x00
BFSR = 0x82
UFSR = 0x0000
HFSR = 0x40000000
DFSR = 0x00000000
MMAR = 0xf0500090
BFAR = 0xf0500090
AFSR = 0x00000000
=======================================================================================================
End Exception
Thanks,