Part Number: TMS570LS1114
I want to check if the target had a hw checking mechanism to check if the entry point 0x00000000 is a valid entry point and if not so we could start from a different entry point
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS1114
I want to check if the target had a hw checking mechanism to check if the entry point 0x00000000 is a valid entry point and if not so we could start from a different entry point
Hi Karim,
I want to check if the target had a hw checking mechanism to check if the entry point 0x00000000 is a valid entry point and if not so we could start from a different entry point
I don't think there was any such mechanism available. I would like to confirm the same with my senior colleague also.
After Power ON Reset the core will directly starts executing the code from 0x00000000 and it won't do any prior validations but there was ECC verification for flash, so any single bit errors or double bit errors in flash can be identified by this SECDED module in controller.
--
Thanks & Regards,
Jagadish.
Hi Karim,
I just got the confirmation!
0x00000000 is the only entry point for TMS570. We don't have such mechanism
—
Thanks & regards,
Jagadish.