Part Number: MCU-PLUS-SDK-AM263X
Other Parts Discussed in Thread: AM2634, UNIFLASH
Hi all,
I'm re-proposing an old question since my issue is still unresolved and the other topic is locked.
I'm trying to test the HS-SE mode features of the AM2634 MCU.
I'm working on an AM263x Control card on which I was able to set the HF-SE mode. I'm using the following libraries:
- MCU_PLUS_SDK_AM263X_09_01_00_41
- OTP_KEYWRITER_AM263X_SR_11_09_01_00_05
- TIFS_AM263X_09_01_00_03
- OpenSSL 1.1.1
I used the following command to generate the keywriter certificate, according to the official documentation:
./gen_keywr_cert.sh -t tifek/am263x/SR_11/ti_fek_public.pem --msv 0x1E22D --msv-protect -b keys_devel/bmpk.pem --bmek keys_devel/bmek.key -b-protect --bmek-protect -s keys_devel/smpk.pem --smek keys_devel/smek.key -s-protect --smek-protect --sr-sbl 1 --sr-hsmRT 1 --sr-app 1 --keycnt 2 --keycnt-protect --keyrev 1 -d am263x --devSrVer SR_11
After running the keywriter on the device, I have the following RBL dump:
---------------------------
SoC ID HW Info:
---------------------------
partID : 0x0
partNumber : 0x2
PGVer : 0x3
ROMVer : 0x2
MetalVer : 0x1
---------------------------
SoC ID R5 ROM Info:
---------------------------
r5 ROM Ver : 0x10100
---------------------------
SoC ID HSM Pub ROM Info:
---------------------------
devName : AM263X
devType : 0xabcd0006 --> HS_SE
hsm ROM Ver : 0x10100
---------------------------
SoC ID HSM Sec ROM Info:
---------------------------
Prime : 0x1
Key Rev : 0x2
Key Count : 0x1
SWRV SBL : 0x1
SWRV HSM : 0x1
TI MPK Hash : ec54cc16cd1ffccab7fd81fd82c998b305c6ac0c12cccf21a610fc1ad7159b1ad20acd69adabf72f1eed15021e26766d2f212d135b6bebf5e5e76c06ac87a6e4
Cust MPK Hash : ce0c44734447afec12ba0b2226c3bdbc15576d212323ece46a9c4ccd6a463e417086083fee572a09a9496dbed447a9f13f9cf535fad75b18e0ee095a4e783c62
Unique ID : a21bf27e0e130cb4ea20898ff70c923779ec1bd222e8aa42243d2422d89f7f609bd30440fcafd1ee1d83912b973702b5a3d756b2bbd246053f6344faf495d954
Now that the card is HS-SE mode, I'm trying to flash my owm SBL.
To do this I built the SBL_UART_UNIFLASH with the following command:
make -s -C examples/drivers/boot/sbl_uart_uniflash/am263x-cc/r5fss0-0_nortos/ti-arm-clang/ all DEVICE=am263x DEVICE_TYPE=HS DEBUG_TIFS=no DEBUG_OPTION=DBG_PUBLIC_ENABLE
After having completed the SBL_UART_UNIFLASH transfer via XMODEM, the MCU stucks and the further SBL code transfer doesn't start as expected.
As suggested on the previous topic, I tried to connect the debug in attach-mode, following this guide.
but the JTAG port remains locked.
Please, can anyone tell me what can be wrong?
Thanks.