This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
This requirement is mainly to deal with post-mass anomalies, you can read the code or save the parameters through the SWD port.
TI-GANG was tried, which could not read even though Unlocking psw was set.
The UniFlash does not see this action.
I wonder if there are any other tools or operation methods and processes that can be introduced?
hello Janz,
yes.I setup SWD password via nonmain memory options, and Program with the MSP-GANG successfully.
then ,I can't "Read" or "Program" through MSP-GANG unless "clear Locked device".
but if "clear Locked device",whole MAIN&NOMAIN memory was be erased.
so I can't get the code with normal operations(GANG or Uniflash).
Thanks
Hello Sanming,
UniFlash and GANG doesn't support SWD password function, but I will tell our software engineer and third party companies to add this function to GANG. And I will give you a script bout this function on UniFlash later.
Best Regards,
Janz Bai
You can refer to this
e2e.ti.com/.../mspm0l1105-recording-the-mspm0l-via-the-command-line
I resolved the issue for now by referring to your response in the following thread: