Hi experts,
Is the CPSW on the TI AM243x, TI AM263x and TI AM263Px same? Are there any differences in the hardware functionality and software offering? Can you please explain the differences in detail.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi experts,
Is the CPSW on the TI AM243x, TI AM263x and TI AM263Px same? Are there any differences in the hardware functionality and software offering? Can you please explain the differences in detail.
Thanks
Hi,
CPSW or Common Platform Switch is a hardware switch providing ethernet functionality to the TI AM2x devices. The AM26x devices carry a 3-port Gigabit CPSW3G subsystem. The 3-port gigabit ethernet subsystem supports two external MAC ports and one internal CPPI (communications port programming interface) or Host port.
The CPSW IP on AM243x andAM263x/AM263Px has different IP versions of the CPSW3G.
Note: The hardware, driver, syscfg and software differences were captured over the MCU_PLUS_SDK 09.02 release. With newer releases, more software examples will be enabled and syscfg differences will be reduced. Check out the release notes of the new SDK versions to get more information.
From software perspective, the offerings for AM243x and AM263x/AM263Px are very similar with a few differences as discussed below:
The syscfg differences are documented below:
Parameter
|
AM243x
|
AM263x/AM263Px
|
---|---|---|
Independently Checksum offload for Rx and Tx |
Cannot be independently disabled
|
Can be independently disabled for Rx and Tx
|
Disable state machine on Open | Planned to be added in future releases |
Supported
|
Monitor PHY addresses | Planned to be added in future releases |
Supported
|
Disable RGMII1 or RGMII2 from syscfg |
Supported
|
Planned to be added in future releases
|
The key enet-cpsw driver differences are documented below:
Parameter
|
AM243x
|
AM263x/AM263Px
|
---|---|---|
Interrupt pacing | Supported via Timer based interrupt pacing | Supported in CPDMA |
Scatter gather | Supported (static memory allocation) | Supported (dynamic memory allocation) |
AutoPHY support | Not supported | Supported |
The key SDK Example differences are documented below:
Parameter
|
AM243x
|
AM263x
|
AM263Px
|
---|---|---|---|
enet_cpsw_fast_startup | Supported | Supported | Planned for future releases |
enet_tx_scatter_gather | Not supported | Supported | Supported |
cpsw_lwip_mqtt | Supported | Supported | Planned for future releases |
Impact of missing software features:
The key hardware differences are documented below:
Feature
|
AM243x
|
AM263x/AM263Px
|
---|---|---|
Per port Castagnoli CRC frame check sequence including host interface for point to point switching, this is negotiated in LLDP to improve protection. | Supported | Limited Support (Host Castagnoli removed for Area) |
Programmable interrupt control with selected interrupt pacing | Not Supported | Supported |
8 Core Support | Not Supported | Supported |
CPPI 3.1 Low cost Multi Channel DMA support up to 8 Cores | Not Supported | Supported |
Streaming Packet Interface support for 64 threads or flows | Supported | Not Supported |
High and low host performance interface options. The High performance mode is used to obtain 40G ingress/egress to the host. | Supported | Not Supported |
MII | Supported | Not Supported (pin limitation) |
SGMII | Supported | Not Supported (requires SERDES) |
ECC rsel | Supported | Not Supported |
TSN/IET - Interspersed Express Traffic (Pre-emption by another name)IEEE802.3br/IEEE802.1Qbu | Supported | Not Supported |
Cut thru switching | Supported | Not Supported |
Number of InterVLAN Routes |
4 | 2 |
DMA engine |
UDMA | CPDMA |
PSIL (Packet Streaming Interface Layer) |
Interfaced with UDMA | CPDMA takes care of the packet streaming between MAC and system memory |
The CPSW MMR registers are also different. For register level changes, please refer to the TRM and register guide of the AM243x, AM263x/AM263Px device.
Note:
Regards,
Shaunak