Part Number: LP-MSPM0L2228
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello,
I'm trying to configure the Timer Capture feature for evaluation for un upcoming project.
The input signal is an external digital signal which stays High when idle, then can trigger commands sendings timed low levels, for example it can stay low for 5 ms, then high 5 ms, and repeat for 5 to 10 times before going back to idle state (high level).
I tried to use pulse-width capture, I can catch the the H->L transition, but I miss the following L->H transition.
I'm trying to configure combined capture, pulse width and period with inverted inputs, but the first low level pulse is not recognized.
Attached you can find syscfg file.
Regards,
Daniele