This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
hi, experts:
I use CCS Theia 1.3.1 and enable hex output, choose Intel hex, then use UniFlash 8.7.0 to flash the hex into the evb, but found it can't power on, can you help to find the cause? Thanks.
Bill
Hi Bill
Could you please comment what evb you used? is it LP-MSPM0C1104: https://www.ti.com/tool/LP-MSPM0C1104 or customized board?
>> but found it can't power on
if you reconnected this board with CCS again, May I know if you can connect, download and debug code using this board?
Thanks
Hi,Xiaodong:
Yes. it is LP-MSPM0C1104, after download the hex, I can't download or debug, only can use CCS to do the factory reset, then it can be download again.
Hi Bill
So, what is the code function? Is this code related with flash operation?
Thanks
hi, Xiaodong:
NO, just simple test of TIMA0, attached is the project along with the hex file.test_tima0.rar