Part Number: TMS570LC4357
Tool/software:
I'm troubleshooting an issue where the ESM High Interrupt (channel 0 in the VIM Init table) is unexpectedly occurring once after any reset, but when I check the ESM Interrupt Offset High Register to determine the reason for the interrupt, its value is 0 (No pending interrupt). What conditions would cause this to happen?
Thanks for any help you can provide.
Cameron