This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello;
I am planning to try ethercat_slave_simple_demo application with AM243x eval board. But firstly, I have a question. ESI files are shared in ESI folder. However, if I want to restructure this ESI file, how will I transfer the updates to the sample code. For example, suppose I generate a new ESI file with Beckhoff SSC tool. I want to move these changes to the code side. How can I do this? Is there a structure that parses ENI file and updates the code?
Thanks
Hi,
You can flash the EEPROM with the updated ESI file in order to reflect the ESI change within the EtherCAT SubDevice. You can refer to the following documentation to flash the updated ESI file to the EEPROM using TwinCAT: Load ESI file to EEPROM
Regards,
Aaron
Hi Aaron;
There are 3 subDevice demos in the SDK that I am interested in. These are SubDevice_Simple, Cia402 and Subdevice Beckhoff SSC. Can I update the ESI file for all 3 examples and flash it to the ESC memory? What is the difference between the Subdevice Beckhoff SSC project and the other 2 projects? Which of these should I use when I start a new project? For the EtherCAT SubDevice Beckhoff SSC Demo project, it is explained how to compile the SDK libraries by downloading the Beckhoff sources. Isn't this also valid for the other demo projects?
Thanks for your support
Kadir
Hi Kadir,
What is the difference between the Subdevice Beckhoff SSC project and the other 2 projects?
Which of these should I use when I start a new project?
Regards,
Aaron
Hi Aaron;
Thank you very much for all sharing.
If I do not have a need that is only covered by Beckhoff SSC, I will prefer to use TI SDK. However, when using TI SDK, I will also need ESI file. I will create this ESI file with Beckhoff SSC Tool and load it into slave device ESC memory. In this way, all ESI variables can be read or parsed by slave application. (by SDK libraries)
Can you please confirm all this information?
Regards
Kadir
Hi Kadir,
For the EtherCAT SubDevice Beckhoff SSC Demo project, it is explained how to compile the SDK libraries by downloading the Beckhoff sources. Isn't this also valid for the other demo projects?
However, when using TI SDK, I will also need ESI file. I will create this ESI file with Beckhoff SSC Tool and load it into slave device ESC memory.
Regards,
Aaron
Hi Kadir,
You can create new ESI by following Steps to Run the Example - Using Beckhoff SSC Tool
Regards,
Aaron