This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G1106: Configuring the clock speed to 32MHz to achieve lower power consumption than 80MHz

Part Number: MSPM0G1106
Other Parts Discussed in Thread: MSPM0L1305, , SYSCONFIG

Tool/software:

Hi,

We're currently using the MSPM0L1305 MCU for our project. Due to the memory restrictions, we are looking to switch to MSPM0G1106.

My question is, with the MSPM0G1106 who's maximum possible clock speed is rated at 80MHz, can we still configure it to run at 32MHz and achieve lower level of power consumption?

I assumed so based on what the datasheet says but wanted to double-check.

Thank you