This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
We're running MSPM0 SDK 2.01.00.03 and would like to start a project using FreeRTOS and TI-Driver Library. We used a similarly named library on the CC1352 with TI-RTOS and SysConfig. This 4-month old thread says SysConfig is not supported, but the UART callback example's README (mspm0_sdk_2_01_00_03/examples/rtos/LP_MSPM0G3507/drivers/uart_callback/README.md) says "SysConfig allows developers to easily configure unused pins by selecting Board→Configure Unused Pins". The example also has source files called ti_drivers_config.c/h which it clearly uses.
Is SysConfig supported on the MSPM0Gxx platform? If not, how do we make use of TI-Driver Library without being able to auto-generate the necessary structs and macro definitions? Is there a recommendation for starting a project with FreeRTOS and using RTOS-safe drivers in general?
Can you clarify how it's supposed to work? I have this warning in SysConfig. Is this my issue?
When I open ti_msp_dl_config.h, I can see that it's generating code based off of my SysConfig selections, but these are different from what the TI-Driver Library calls expect.
/* * Copyright (c) 2023, Texas Instruments Incorporated - http://www.ti.com * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* * ============ ti_msp_dl_config.h ============= * Configured MSPM0 DriverLib module declarations * * DO NOT EDIT - This file is generated for the MSPM0G110X * by the SysConfig tool. */ #ifndef ti_msp_dl_config_h #define ti_msp_dl_config_h #define CONFIG_MSPM0G110X #if defined(__ti_version__) || defined(__TI_COMPILER_VERSION__) #define SYSCONFIG_WEAK __attribute__((weak)) #elif defined(__IAR_SYSTEMS_ICC__) #define SYSCONFIG_WEAK __weak #elif defined(__GNUC__) #define SYSCONFIG_WEAK __attribute__((weak)) #endif #include <ti/devices/msp/msp.h> #include <ti/driverlib/driverlib.h> #include <ti/driverlib/m0p/dl_core.h> #ifdef __cplusplus extern "C" { #endif /* * ======== SYSCFG_DL_init ======== * Perform all required MSP DL initialization * * This function should be called once at a point before any use of * MSP DL. */ /* clang-format off */ #define POWER_STARTUP_DELAY (16) #define CPUCLK_FREQ 80000000 /* Defines for UART_RS485 */ #define UART_RS485_INST UART0 #define UART_RS485_INST_IRQHandler UART0_IRQHandler #define UART_RS485_INST_INT_IRQN UART0_INT_IRQn #define GPIO_UART_RS485_RX_PORT GPIOA #define GPIO_UART_RS485_TX_PORT GPIOA #define GPIO_UART_RS485_RX_PIN DL_GPIO_PIN_1 #define GPIO_UART_RS485_TX_PIN DL_GPIO_PIN_0 #define GPIO_UART_RS485_IOMUX_RX (IOMUX_PINCM2) #define GPIO_UART_RS485_IOMUX_TX (IOMUX_PINCM1) #define GPIO_UART_RS485_IOMUX_RX_FUNC IOMUX_PINCM2_PF_UART0_RX #define GPIO_UART_RS485_IOMUX_TX_FUNC IOMUX_PINCM1_PF_UART0_TX #define UART_RS485_BAUD_RATE (5000000) #define UART_RS485_IBRD_40_MHZ_5000000_BAUD (1) #define UART_RS485_FBRD_40_MHZ_5000000_BAUD (0) /* clang-format on */ void SYSCFG_DL_init(void); void SYSCFG_DL_initPower(void); void SYSCFG_DL_GPIO_init(void); void SYSCFG_DL_SYSCTL_init(void); void SYSCFG_DL_SYSCTL_CLK_init(void); void SYSCFG_DL_UART_RS485_init(void); bool SYSCFG_DL_saveConfiguration(void); bool SYSCFG_DL_restoreConfiguration(void); #ifdef __cplusplus } #endif #endif /* ti_msp_dl_config_h */
The ti_drivers_config.h file from the UART example is:
/* * Copyright (c) 2021, Texas Instruments Incorporated - http://www.ti.com * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* * ============ ti_drivers_config.h ============= * Configured MSPM0 Driver module declarations * * DO NOT EDIT - This file is generated for the LP_MSPM0G3507 * by the SysConfig tool. */ #ifndef ti_drivers_config_h #define ti_drivers_config_h #define CONFIG_LP_MSPM0G3507 #if defined(__ti_version__) || defined(__TI_COMPILER_VERSION__) #define SYSCONFIG_WEAK __attribute__((weak)) #elif defined(__IAR_SYSTEMS_ICC__) #define SYSCONFIG_WEAK __weak #elif defined(__GNUC__) #define SYSCONFIG_WEAK __attribute__((weak)) #endif #include <stdio.h> #include <ti/devices/msp/msp.h> #include <ti/driverlib/driverlib.h> #include <ti/driverlib/m0p/dl_core.h> #include <ti/drivers/UART.h> #include <ti/drivers/dma/DMAMSPM0.h> #include <ti/drivers/uart/UARTMSPM0.h> #define CONFIG_UART_COUNT 1 #define CONFIG_UART_BUFFER_LENGTH 1 #define CONFIG_DMA_COUNT 1 #define CONFIG_DMA_CH_COUNT 1 #define DEFAULT_DMA_PRIORITY 31 extern const uint_least8_t CONFIG_UART_0; extern const uint_least8_t UART_count; uint8_t rxBuffer[CONFIG_UART_BUFFER_LENGTH]; uint8_t txBuffer[CONFIG_UART_BUFFER_LENGTH]; /* clang-format on */ void UART0_IRQHandler(void); /* * ======== SYSCFG_DL_init ======== * Perform all required MSP DL initialization * * This function should be called once at a point before any use of * MSP DL. */ /* clang-format off */ /* Defines for CONFIG_UART_0 */ #define CONFIG_UART_0_INST UART0 #define CONFIG_UART_BAUD_RATE (115200) /* Port definition for Pin Group GPIO_GRP_0 */ #define GPIO_GRP_0_PORT (GPIOA) /* Defines for PIN_0: GPIOA.0 with pinCMx 1 on package pin 33 */ #define GPIO_GRP_0_PIN_0_PIN (DL_GPIO_PIN_0) #define GPIO_GRP_0_PIN_0_IOMUX (IOMUX_PINCM1) /* clang-format on */ #endif /* ti_drivers_config_h */
The UART example calls this to open the UART handle and passes a const uint_least8_t. These don't exist in the ti_msp_dl_config.h from above.
extern const uint_least8_t CONFIG_UART_0; uart = UART_open(CONFIG_UART_0, &uartParams);
I can see that it generates initialization calls (SYSCFG_DL_*) for everything I configured. This is different form the UART example. I'm not sure how to use this with TI-Driver Library. What am I doing wrong?
I just found this recent thread: https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1356956/mspm0g3507-ti_drivers_config-c-not-generated-by-sysconfig. Is this still true that it only works for the low-level DriverLib and not the thread-safe TI-Drivers? If so, this is a large hole if we're to move to the M0 platform.
Hi,
Only ti_msp_dl_config.h/c will be generated by Sysconfig using driverlib file.
And ti_drivers_config.c/h use TI-_drivers.
To use sysconfig, please add Sysconfig into Products. And you can find auto-generated file in Debug file. Please remember to remove the old one.
Also, you can refer to below demo code:
...\examples\rtos\LP_MSPM0G3507\kernel\blink_led
Regards,
Zoey