Part Number: AM2634-Q1
Tool/software:
Hi,
Have a query related to external Watchdog when we use TPS653860A-Q1 with AMS2634-Q1.
1. Can we keep refreshing the external WD over SPI from cluster 0 (core 0 and 1 in lockstep) and cluster 1 (core 2 and core 3 in lockstep ) in windowed WD?
2. If yes, In case cluster 1 is stuck and not able to refresh external WD, cluster2 can continue refreshing the WD and allow the micro to run
Regards
Sunil