Part Number: LP-AM243
Other Parts Discussed in Thread: AM2434
Tool/software:
Dear Specialists,
I have a AM243X-LP demo-board. I successfully did "Flash SOC Initialization binary" on the AM243X-LP demo-board.
According to AM243X MCU+ SDK 10.00.00 "Getting Started" chapter's "EVM Setup" section, the next step is "SOC Initialization Using CCS Scripting".
I set the path to the SDK. The next step is to "Create Target Configuration" and "Launch Selected Configuration".
With the help of Mr. Tushar Thakur, I successfully created a "New TargetConfiguration".
On the EVM Setup section inside AM243x MCU+ SDK 10.00.00, the next step is to "Run the SOC Initialization Script" on the AM243X-LP section.
In this section, I setup the BOOTMODE 1-8(SW4) and then power on the AM243X-LP and then Launch Selected Configuration and I saw the "Debug" window appeared correctly.
On the next step is to run a script. But I couldn't get that script to finish successfully.
The error information in right hand side Scripting Console is as following (the left hand side Console has some completed echo message):

Can anybody help me to find out where was wrong to cause this fail.
Thank you very much.
Best Regards,
Jason Chiu.