Part Number: RM57L843
Tool/software:
Hi,
I am trying to use CRC on RM57. The structure passed to crcSignGen has "src_data_pat" whhich is a pointer to a buffer with 64 bit data buffer and another field is "data_length" which is number of 64 bit sized words in src_data_pat. However, if say I only have 5 bytes of data, what shoukd each of these values be?
Also, I tried the following code with a 64 bit data and I am getting wrong CRC value. Could you any tell me if I am missing something? I have configured this in FULL_CPU mode and using CRC1 and channel 0.
crcModConfig_t param;
uint64_t data = 0x4142434445464748;
void main()
{
crcInit();
crcChannelReset(crcREG1, 0);
param.crc_channel = 0;
param.mode = CRC_FULL_CPU;
param.data_length = 1;
param.src_data_pat = &data;
crcSignGen(crcREG1, ¶m);
sig = crcGetSectorSig(crcREG1, 0);
}
The value I am getting is 0xB19C8742DDF0EBAA whereas the correct value is 0x38178634E55140F2.
Thanks,
Ravi