Part Number: MSPM0G1107
Other Parts Discussed in Thread: MSPM0L1117, LP-MSPM0G3507
Tool/software:
Dear Support Team,
I have a question regarding above ERRATA ADC_ERR_06. We have several customer Boards, power supply of controller is 3.0V Analog Reference Voltage is 2.5V external.
Samping Rate is 6MHz @12Bit resolution.
Some of our Boards have the subscribed Phenomens in the ERRATA of TI. Some ot them not, even the phenomen seems to disappear when we increase the supply voltage to 3.3V.
Additional nearly same Software runs on Eval Board of TI, with never seen this 0x800 Phenomen.
Could it be that an increase of the supply Voltage to 3.3V solve this Issue?
Will the problem disappear by reducing ADC resolution ton 10Bit?
Because sugggested workarounds in ERRATA are all not acceptable for our product.
We have to read out the DMA with 100KHz and do some calculations, no real remaining CPU Power. Additionally the value 0x800 could be a real analog value in our application.
We activated already the averaging function but it helps only to reduce the problem. Not really a solution.
We will be happy for every information you share with us.
If you can't provide a real solution, will there be a new silicon revision possible?
If not I fear our work would end up in much wasted time.
Best regards
Siegfried