Tool/software:
Hi TI Experts,
Customer is working on SDK9.2.
They recently meet a strange problem when Ethercat upgrade in flash.
If the UART DMA is enabled (non-cacheable) when Ethercat upgrade, write value 1 to the flash address 0x7e000, the read out value at the same flash address is 0 not expected 1. The same situations happens for writing many other address in the flash also.
If the UART DMA is disabled when Ethercat upgrade, write value 1 to the flash address 0x7f000, the read out value at the same flash address is 1 as expected. And it is working in all other address writing.
This really confuse customer how the UART DMA could somehow affect the ethercat flashing values.
The UART Transfer coding is below.
The UART Receiver coding is below.
Could you help provide some suggestions please?
Thanks,
Kevin
How are they flashing ? Using MCU+ SDK McSPI or OSPI driver ? May be something to do with CBASS QoS settings. Can they reproduce without EtherCAT ? It works when UART is used without DMA ?
Hi Pratheesh,
Thanks for your reply.
Customer is using OSPI driver. If not using EtherCat, then it is hard to reproduce this problem.
It works normally if UART is used without DMA.
May I know could you share some guide with CBASS QoS settings please?
Thanks,
Kevin
Hi Kevin,
We'll check on this and get back to you by EOD today. Thank you for your patience.
Regards,
Aaron
Hi Aaron,
This seems a system level problem. Customer previously only used R5f0_0 SOP last year. And in that project customer also used Ethercat upgrade in flash, and they could also use UART DMA at the same time. The new project involves additional R5f1_0 core, and additional UART ports & IPC communication is introduced associated with R5f1_0. At this moment, if customer disable DMA in the UART it is still working normally, but will have the above problem if DMA is enabled.
Could you firstly share some guidance of CBASS QoS settings for customer to have a try?
Thanks,
Kevin
Hi Kevin,
Can the customer share the interrupt and task priorities? We suspect if the higher priority task/interrupt is preempting the Flash read task.
Regards,
Aaron
Hi Aaron,
The tasks running apart from Ethercat flashing are IPC communication & UART DMA. We are not quite sure how to look at the priorities, but customer provided the syscfg files below, so maybe you could more conveniently look at it.
FIOB -> R50-0
FIOB_CHA_Safety -> R51-0
Thanks,
Kevin
If the UART DMA is enabled (non-cacheable)
Hello Kevin,
Do we get a customer application to look at the total application ?
What is the meaning of UART DMA being non-cacheble , which means the buffer that is used for UART communication is kept then as non-cacheble?
If UART buffets are non-cacheble, then why user use Cache_wb and Cache_Inv API's in the above attached images ?
Can you also please confirm whether the source buffer and destination buffers belong to flash memory or which memory is used ?
Is there any connection between the IPC , Ethercat, UART and flash, like sharing Ethercat buffets for flash writing or reading or similarly to use for UART DMA?
Can you please share the task details for UART DMA ?
What are the priorities for all the tasks ?
Regards,
Anil.
Hi Anil,
If UART buffets are non-cacheable, then why user use Cache_wb and Cache_Inv API's in the above attached images ?
Customer feedback: We just directly use the default SDK configurations according to the uart dma demo, we did not intentionally configure them. If you think the default Cache_wb and Cache_Inv API will make UART buffer become cacheable, then we could do an experiment to remove them.
Is there any connection between the IPC , Ethercat, UART and flash, like sharing Ethercat buffets for flash writing or reading or similarly to use for UART DMA?
Customer feedback: No, they are all independent. And only Ethercat task will read/write flash. And only UART will configure DMA.
What are the priorities for all the tasks ?
Customer feedback:
Uart
IPC
Ethercat
Can you also please confirm whether the source buffer and destination buffers belong to flash memory or which memory is used?
Customer Feedback:
UART: buffer is used
IPC: buffer is used
Ethercat read/write flash: buffer is used
Do we get a customer application to look at the total application?
Can you please share the task details for UART DMA?
Customer feedback: We could only provide UART DMA case details below.
#define CRC_START_VALUE (0x00) #define CHB_PROXY_TASK_STACK_SIZE (1024 * 4) #define CHB_PROXY_TASK_PRIORITY (4U) #define CHB_META_PACKAGE_BYTES_NUM (4U) #define CHB_FRAME_LENGTH_MAX_BYTES_NUM (255U) #define CHA_ACK_NACK_PACKAGE_BYTES_NUM (4U) #define CHA_ACK_HEADER (0x51) #define CHA_NACK_HEADER (0x52) #define CHB_CONTENT_PACKAGE_HEADER (0xA2) // MAIN_DEG_UART0 is used in DIOB/EIOB for testing. // MAIN_ADCIF_UART4 is used in FIOB for development. #define CHB_PROXY_TASK_UART_TRANS_INDEX (MAIN_ADCIF_UART4) // #define CHB_PROXY_TASK_UART_DMA_STATUS (true) #define CHB_ADC_CONTENT_LENGTH (8U) // In bytes. #define CHB_TEMP_CONTENT_LENGTH (1U) #define CHB_GPIO_CONTENT_LENGTH (1U) #define CHB_UART_STATUS_CONTENT_LENGTH (3U) #define CHB_SPI_STATUS_CONTENT_LENGTH (1U) /*****************************[TYPE DEFINE]***********************************************/ typedef enum { RESERVED_CHA_ERR = 0x01, RESERVED_META_PACKAGE_CRC_ERR, RESERVED_CONTENT_PACKAGE_CRC_ERR, }ReservedInfo; //These are the specified information of type-INFO_RESERVED. typedef enum { FRAME_HEADER_ERR = 0x01, FRAME_CRC_ERR, }FrameErrInfo; //These are the specified information of type-INFO_FRAME_ERROR. typedef enum { INFO_RESERVED = 0x01, INFO_FRAME_ERROR, INFO_CHB_ADC = 0x10, INFO_CHB_TEMP, INFO_CHB_GPIO, INFO_CHB_UART_STATUS, INFO_CHB_SPI_STATUS, INFO_LOG = 0xFF, }SInfoType; typedef enum { ACK_HEADER = 0, ACK_TYPE, ACK_ERR_INFO, ACK_CRC, ACK_PACKAGE_NUM, }EAckPackage; typedef enum { META_HEADER = 0, META_LENGTH, META_CRC = 3, }EMetaPackage; typedef enum { CONTENT_HEADER = 0, CONTENT_FRAMENUM, CONTENT_CRC, CONTENT_FIRST_FRAME_TYPE, }EContentPackage; typedef struct { uint8_t contentPackage[UART_MAX_BUFSIZE]; // bool errOccur; // Mask the error occurred status in "content package receive" or "content package parse and distribute" phase. uint16_t contentLength; // In bytes, which included header, frame number, CRC, FrameX... }SContentPackageInfo; typedef struct { // bool errOccur; uint8_t ackPackage[CHA_ACK_NACK_PACKAGE_BYTES_NUM*8]; uint8_t nackPackage[CHA_ACK_NACK_PACKAGE_BYTES_NUM*8]; bool errOccur; }SAtoBPackageInfo; typedef struct { uint32_t ChbAdcVal[2]; // Element 0 for ADC CH0; Element 1 for ADC CH1. uint8_t ChbTempVal; uint8_t ChbGpioState; // Bit0 - IN_MSPM0_SPI_BUSY; // Bit1 - IN_MSPM0_REQ_FW; // Bit2 - IN_SS_SIN_1_A; // Bit3 - IN_SS_SPARE0_A; // Bit4 - IN_SIN_0_A; uint8_t ChbUartStatus[3]; // Element 0 for Uart0... uint8_t ChbSpiStatus; }SChbInfo; typedef enum { UART_ST_CLEAR = 0, META_REV_AND_CHECK, NACK_SEND, CONTENT_REV_START_ACK_SEND, CONTENT_CHECK, CHB_PROXY_STATE_NUM, }EChBProxyState; typedef struct { EChBProxyState currentState; EChBProxyState (* stateAction)(void); // Return value is the next state. }SChBProxyStMachine; /***********************[System-global Variables]******************************/ static uint32_t gChbProxyTaskStack[CHB_PROXY_TASK_STACK_SIZE/sizeof(uint32_t)] __attribute__((aligned(32))); static TaskP_Object ChBProxyTaskObject; static SContentPackageInfo cpHandler __attribute__((aligned(32))) = {.contentLength = 0, .contentPackage={0}}; static uint8_t metaPackage[CHB_META_PACKAGE_BYTES_NUM*8] __attribute__((aligned(32))); static SAtoBPackageInfo aTobPackage __attribute__((aligned(32))) = {.errOccur = false, }; extern UART_Handle gUartHandle[CONFIG_UART_NUM_INSTANCES]; static uint16_t uartStatus = 0xFFU; static SChbInfo chbInfo = { .ChbAdcVal = {0xff, 0xff}, .ChbTempVal = 0xff, .ChbGpioState = 0xff, .ChbUartStatus = {0xff, 0xff, 0xff}, .ChbSpiStatus = 0xff, }; static SemaphoreP_Object gReadDoneSem; static SemaphoreP_Object gWriteDoneSem; static EChBProxyState chbProxyCurrentState = UART_ST_CLEAR; /***********************[STATIC FUNCTION]**************************************/ static void set_mainUart4Status(uint16_t statusValue); static void ChBProxyTask_Main(void *argument); static void parseDistribute(void); static EChBProxyState clearUartAct(void); static EChBProxyState metaRevAndCheckAct(void); static EChBProxyState nackSendAct(void); static EChBProxyState contentRevStartAckSendAct(void); static EChBProxyState contentCheckAct(void); static SChBProxyStMachine chBProxyStateMachine[CHB_PROXY_STATE_NUM] = { {UART_ST_CLEAR, clearUartAct}, {META_REV_AND_CHECK, metaRevAndCheckAct}, {NACK_SEND, nackSendAct}, {CONTENT_REV_START_ACK_SEND, contentRevStartAckSendAct}, {CONTENT_CHECK, contentCheckAct}, }; void ChBProxyTask_Init(void) { TaskP_Params taskParams; uint32_t status = SystemP_FAILURE; // Uart initialization Uart_Init(); status = SemaphoreP_constructBinary(&gReadDoneSem, 0); DebugP_assert(SystemP_SUCCESS == status); status = SemaphoreP_constructBinary(&gWriteDoneSem, 0); DebugP_assert(SystemP_SUCCESS == status); TaskP_Params_init(&taskParams); taskParams.name = "ChBProxyTask"; taskParams.stackSize = CHB_PROXY_TASK_STACK_SIZE; taskParams.stack = (uint8_t*) gChbProxyTaskStack; taskParams.priority = CHB_PROXY_TASK_PRIORITY; taskParams.taskMain = (TaskP_FxnMain) ChBProxyTask_Main; status = TaskP_construct(&ChBProxyTaskObject, &taskParams); DebugP_assert(status == SystemP_SUCCESS); KUKA_log("[UART4] CHB PROXY TASK initialization done\r\n"); } void get_mainUart4Status(uint16_t * const pStatus) { portENTER_CRITICAL(); *pStatus = uartStatus; portEXIT_CRITICAL(); } void get_chbAdcVal(uint32_t * const pChbAdc, uint8_t adcIndex) { portENTER_CRITICAL(); *pChbAdc = chbInfo.ChbAdcVal[adcIndex]; portEXIT_CRITICAL(); } void get_chbTempVal(uint8_t * const pChbTemp) { portENTER_CRITICAL(); *pChbTemp = chbInfo.ChbTempVal; portEXIT_CRITICAL(); } void get_chbGpioVal(bool * const pGpioVal, EChbGpioIndex gpioIndex) { bool gpioVal = (chbInfo.ChbGpioState&(0x1<<gpioIndex)) >> gpioIndex; portENTER_CRITICAL(); *pGpioVal = gpioVal; portEXIT_CRITICAL(); } void get_chbUartSt(uint8_t * const pUartSt, EChbUartIndex uartIndex) { portENTER_CRITICAL(); *pUartSt = chbInfo.ChbUartStatus[uartIndex]; portEXIT_CRITICAL(); } void get_chbSpiSt(uint8_t * const pSpiSt) { portENTER_CRITICAL(); *pSpiSt = chbInfo.ChbSpiStatus; portEXIT_CRITICAL(); } static void set_mainUart4Status(uint16_t statusValue) { static bool firstTimeSet = true; portENTER_CRITICAL(); if(firstTimeSet) { uartStatus = 0x00U; firstTimeSet = false; } uartStatus |= statusValue; portEXIT_CRITICAL(); } static void ChBProxyTask_Main(void *argument) { while (1) { // while(APPL_IsBootMode()) // { // ClockP_usleep(1000*1000); // } chbProxyCurrentState = chBProxyStateMachine[chbProxyCurrentState].stateAction(); } } static EChBProxyState clearUartAct(void) { int32_t ret = SystemP_SUCCESS; UART_Config *config; config = (UART_Config *)gUartHandle[CHB_PROXY_TASK_UART_TRANS_INDEX]; // Clear chb Proxy false flag. aTobPackage.errOccur = false; // Clear the UART status. ret = UART_procLineStatusErr((UARTLLD_Handle)(config->object->uartLld_handle)); if(SystemP_SUCCESS != ret) { // Return the channel A error to B side. aTobPackage.errOccur = true; aTobPackage.nackPackage[ACK_HEADER] = CHA_NACK_HEADER; aTobPackage.nackPackage[ACK_TYPE] = INFO_RESERVED; aTobPackage.nackPackage[ACK_ERR_INFO] = RESERVED_CHA_ERR; aTobPackage.nackPackage[ACK_CRC] = CRC_CalCrc8(aTobPackage.nackPackage, 3, CRC_START_VALUE); KUKA_log("[UART4] UART4 clear status fail: %d.\r\n", ret); } // Change to next state. return META_REV_AND_CHECK; } static EChBProxyState metaRevAndCheckAct(void) { int32_t receiveSt; uint8_t metaCrc = 0; EChBProxyState nextState; // Uart receive: Header 0xA1 receiveSt = Uart_Receive(CHB_PROXY_TASK_UART_TRANS_INDEX, &metaPackage, CHB_META_PACKAGE_BYTES_NUM); // Waiting for meta package receive done. SemaphoreP_pend(&gReadDoneSem, SystemP_WAIT_FOREVER); if(receiveSt != SystemP_SUCCESS) { // Set MAIN UART4 status for FCT test. KUKA_log("[UART4] UART4 meta package receive fail: %d.\r\n", receiveSt); set_mainUart4Status(0x02U); // Return the channel A error to B side. aTobPackage.errOccur = true; aTobPackage.nackPackage[ACK_HEADER] = CHA_NACK_HEADER; aTobPackage.nackPackage[ACK_TYPE] = INFO_RESERVED; aTobPackage.nackPackage[ACK_ERR_INFO] = RESERVED_CHA_ERR; aTobPackage.nackPackage[ACK_CRC] = CRC_CalCrc8(aTobPackage.nackPackage, 3, CRC_START_VALUE); } else { // Set MAIN UART4 status for FCT test. set_mainUart4Status(0x00U); // CRC8 for package which header is 0xA1. metaCrc = CRC_CalCrc8(metaPackage, 3, CRC_START_VALUE); if(metaCrc == metaPackage[META_CRC]) { aTobPackage.ackPackage[ACK_HEADER] = CHA_ACK_HEADER; aTobPackage.ackPackage[ACK_TYPE] = 0x00; aTobPackage.ackPackage[ACK_ERR_INFO] = 0x00; aTobPackage.ackPackage[ACK_CRC] = CRC_CalCrc8(aTobPackage.ackPackage, 3, CRC_START_VALUE); // Store packageLen; memcpy(&cpHandler.contentLength, &metaPackage[META_LENGTH], 2); DebugP_assert(cpHandler.contentLength <= UART_MAX_BUFSIZE); // Stop the process when the content length is larger than the UART_MAX_BUFSIZE. } else { // Return the CRC error information to B side. aTobPackage.errOccur = true; aTobPackage.nackPackage[ACK_HEADER] = CHA_NACK_HEADER; aTobPackage.nackPackage[ACK_TYPE] = INFO_RESERVED; aTobPackage.nackPackage[ACK_ERR_INFO] = RESERVED_META_PACKAGE_CRC_ERR; aTobPackage.nackPackage[ACK_CRC] = CRC_CalCrc8(aTobPackage.nackPackage, 3, CRC_START_VALUE); KUKA_log("[UART4] Meta package CRC fail.\r\n"); } } if(aTobPackage.errOccur) { return NACK_SEND; } return CONTENT_REV_START_ACK_SEND; } static EChBProxyState nackSendAct(void) { int32_t ret = SystemP_SUCCESS; // When there is an error, transfer the nack package to B side. ret = Uart_Transfer(CHB_PROXY_TASK_UART_TRANS_INDEX, aTobPackage.nackPackage, ACK_PACKAGE_NUM); // Waiting for transfer done. SemaphoreP_pend(&gWriteDoneSem, SystemP_WAIT_FOREVER); if(ret != SystemP_SUCCESS) { // Set MAIN UART4 status for FCT test. KUKA_log("[UART4] UART4 transfer fail: %d.\r\n", ret); set_mainUart4Status(0x01U); } else { // Set MAIN UART4 status for FCT test. set_mainUart4Status(0x00U); } return UART_ST_CLEAR; } static EChBProxyState contentRevStartAckSendAct(void) { int32_t ret; // Start content package receive(Prepare for content package DMA) Uart_Receive(CHB_PROXY_TASK_UART_TRANS_INDEX, cpHandler.contentPackage, cpHandler.contentLength); // Send ACK ret = Uart_Transfer(CHB_PROXY_TASK_UART_TRANS_INDEX, aTobPackage.ackPackage, ACK_PACKAGE_NUM); // Waiting for transfer done. SemaphoreP_pend(&gWriteDoneSem, SystemP_WAIT_FOREVER); if(ret != SystemP_SUCCESS) { // Set MAIN UART4 status for FCT test. KUKA_log("[UART4] UART4 transfer fail: %d.\r\n", ret); set_mainUart4Status(0x01U); return UART_ST_CLEAR; // If ACK send fail, return UART_ST_CLEAR state. } else { // Set MAIN UART4 status for FCT test. set_mainUart4Status(0x00U); } return CONTENT_CHECK; } static EChBProxyState contentCheckAct(void) { // Waiting for meta package receive done. SemaphoreP_pend(&gReadDoneSem, SystemP_WAIT_FOREVER); // Content package CRC check for the front second bytes. If fail, ignore this content package and start the next cycle. if(CRC_CalCrc8(cpHandler.contentPackage, 2, CRC_START_VALUE) != cpHandler.contentPackage[CONTENT_CRC]) { KUKA_log("[UART4] Content package CRC fail.\r\n"); return UART_ST_CLEAR; } else { // Parse and contribute the content package message. parseDistribute(); } return UART_ST_CLEAR; } static void parseDistribute(void) { uint8_t crcVal = 0; uint8_t curFrameIndex, nextFrameIndex; uint8_t curFrameType, curFrameLength; uint8_t curFrameContent[CHB_FRAME_LENGTH_MAX_BYTES_NUM]; uint8_t frameCrc = 0; if(cpHandler.contentPackage[CONTENT_HEADER] == CHB_CONTENT_PACKAGE_HEADER) { // Get the first frame's type and length. curFrameIndex = CONTENT_FIRST_FRAME_TYPE; // Content package prase and distribute. for(uint8_t i = 0; i < cpHandler.contentPackage[CONTENT_FRAMENUM]; i++) { curFrameType = cpHandler.contentPackage[curFrameIndex]; curFrameLength = cpHandler.contentPackage[curFrameIndex+1]; // Calculate next frame index in content Package. nextFrameIndex = curFrameIndex+curFrameLength+3; // Calculate current frame CRC value. If CRC fail, ignore current frame. frameCrc = CRC_CalCrc8(&cpHandler.contentPackage[curFrameIndex], curFrameLength+2, CRC_START_VALUE); if(frameCrc == cpHandler.contentPackage[nextFrameIndex-1]) { // Prase current frame content package. memcpy(curFrameContent, &(cpHandler.contentPackage[curFrameIndex+2]), curFrameLength); // Package value distribute according to the frame type. switch(curFrameType) { // Switch Case from "SInfoType" case INFO_CHB_ADC: // function to send the content package "curFrameContent" to related module. portENTER_CRITICAL(); memcpy(&chbInfo.ChbAdcVal[1], &curFrameContent[0], CHB_ADC_CONTENT_LENGTH/2); memcpy(&chbInfo.ChbAdcVal[0], &curFrameContent[4], CHB_ADC_CONTENT_LENGTH/2); portEXIT_CRITICAL(); break; case INFO_CHB_TEMP: // function to send the content package "curFrameContent" to related module. portENTER_CRITICAL(); memcpy(&chbInfo.ChbTempVal, curFrameContent, CHB_TEMP_CONTENT_LENGTH); portEXIT_CRITICAL(); break; case INFO_CHB_GPIO: portENTER_CRITICAL(); memcpy(&chbInfo.ChbGpioState, curFrameContent, CHB_GPIO_CONTENT_LENGTH); portEXIT_CRITICAL(); break; case INFO_CHB_UART_STATUS: portENTER_CRITICAL(); memcpy(&chbInfo.ChbUartStatus, curFrameContent, CHB_UART_STATUS_CONTENT_LENGTH); portEXIT_CRITICAL(); break; case INFO_CHB_SPI_STATUS: portENTER_CRITICAL(); memcpy(&chbInfo.ChbSpiStatus, curFrameContent, CHB_SPI_STATUS_CONTENT_LENGTH); portEXIT_CRITICAL(); break; case INFO_LOG: // write to LittleFS, remove null added by DebugP_shmLogReaderGetString KUKA_slog((const char *)curFrameContent, curFrameLength-1); break; default: break; } } curFrameIndex = nextFrameIndex; } } } void adcIfUart_readDoneCb(void) { SemaphoreP_post(&gReadDoneSem); } void adcIfUart_writeDoneCb(void) { SemaphoreP_post(&gWriteDoneSem); }
Thanks,
Kevin
Hello Kevin,
Can you please confirm the Ethercat and other tasks are running ?
I suspect that the UART with DMA task creates an issue, and already you have confirmed that the same code without DMA enablement is functioning.
So, this might be a problem with the UART DMA task and when this task is running and the Ethercat task is not able to write data on the Flash memory.
That's the reason we are able to see content on the flash memory is always zero.
Can you please confirm whether all tasks are running or not ?
Try another test. There is UART_DMA transfer API comment out and verify the same test case .
Regards,
Anil.
Hi Anil,
If customer comment out both UART_DMA transfer & receive API, then the Ethercat upgrade read/write in flash becomes normal.
So that means the root cause comes from UART_DMA transfer & receive API, may I know what could be the next step to debug?
Thanks,
Kevin
Hello Kevin,
Yes, the above two APIs seems are the culprit.
I am not sure what is going on in the customer application when calling UART DMA TX and UART DMA RX APIs.
I need the reproducible code on the EVM to debug further. Otherwise, it is very difficult to debug further.
After calling the UART DMA TX and UART DMA RX, check if the RTOS timer interrupt is coming or not.
Can you please confirm the break points in all the tasks and see if tasks are hit or not after the UART DMA TX/RX API is called?
This gives information about whether all tasks are suspended or not.
Regards,
Anil.
Hi Anil,
As discussed offline, customer could continuously see the Ethercat log when Uart DMA is enabled, which means the Ethercat task is running actually.
It is not that easy to create task reproducing on EVM for a short time. Customer previously only used R5f0_0 SOP last year. And in that project customer also used Ethercat upgrade in flash, and they could also use UART DMA at the same time. The new project involves additional R5f1_0 core, and additional UART ports & IPC communication is introduced associated with R5f1_0. At this moment, if customer disable DMA in the UART it is still working normally, but will have the above problem if DMA is enabled.
May I know based on the above UART coding & QoS setting, could we have any other things for customer to have a try?
Thanks,
Kevin
Hello Kevin,
I discussed offline with Kevin and Kevin will share all customer project details further to debug the issue.
Regards,
Anil.
Hi Anil,
I listed the details for R5F0_0 and R5f1_0 below.
R5F0_0
1: Ethercat upgrade flash, using SDK default OSPI driver (DMA disabled). The Ethercat writes data to on-chip RAM firstly, and then R5F0_0 read from the on-chip ram and write to the flash, not using IPC shared data.
2: UART (DMA enabled). This UART will print the log for R5F1_0 also, the R5F1_0 will put the log into the shared memory, and then R5F0_0 will read the log and print it out using this UART.
3: IPC with R5F1_0
4: Timer
R5F1_0
1: UART (DMA disabled)
2: IPC with R5F0_0
For the last year project, customer only used R5F0_0, and there is no problem. This year new project introduced the R5F1_0, and the overall system will occur this problem.
Customer has mentioned that they have tried to avoid the on-chip ram overlap for different tasks by setting different buffer shown below (you could refer to the previous reply which has this information).
Thanks,
Kevin
Hello Kevin,
Please try the following test cases:
Test Case 1: Swap Task Priorities
In the customer application, the following task priorities are currently configured:
• UART Task Priority: 4
• EtherCAT (OSPI Write) Task Priority: 2
Modify the configuration as below:
• Set UART Task Priority to 2
• Set EtherCAT Task Priority to 4
Test Case 2: Buffer Memory Placement
In the customer application, both UART and EtherCAT tasks are using MSRAM to write data to OSPI, with DMA handling the data transfers.
To evaluate the impact of memory access latency and bus contention, try the following:
• Move one of the buffers from MSRAM to TCM:
• Option A: Place the UART TX/RX DMA buffer in TCM
• Option B: Place the OSPI Write/Read buffer in TCM
Test Case 3: UART DMA Frequency
Check how frequently UART DMA is being triggered in the application.
Example:
• Currently, UART DMA is triggered every 1 ms
• Modify this to 100 ms and observe the behavior
Regards,
Anil.
Hi Anil,
Please see the result of the above 3 test cases, thanks.
Test Case 1: Swap Task Priorities
Modification
Result
This UART operates as a slave, connected to an external UART master device. The master device continuously sends data every 10ms. However, the priority level of the UART task is set too low, causing the receive buffer to overflow. This results in error reports and triggers a watchdog timeout reset due to unprocessed data.
Test Case 2: Buffer Memory Placement
Modification
Result
After modifying the UART buffer under TCMA, the data read from it is all incorrect for some unknown reason.
Test Case 3: UART DMA Frequency
Modification
Result
This UART is configured as a slave and connected to an external UART master device. The master device continuously transmits data every 10ms without interruption. Due to the slow processing speed of the UART task, the receive buffer becomes full, triggering errors and causing a watchdog timeout reboot.
Any clue you could find in the test results?
Thanks,
Kevin
Hello Kevin,
The above results are not as expected.
I need to do analysis on these test cases.
Meanwhile, please share the exact steps the customer did, and I need to review the code changes as well.
Regards,
Anil.