Tool/software:
Hello,experts
I would like to follow up on this thread with a question
If I don't check the box [Disable Auth For Application Image], there is a status = SystemP_FAILURE from Bootloader_parseMultiCoreAppImage(bootHandle, &bootImageInfo);
but, if I check the box [Disable Auth For Application Image], there is also a status that the app cann't run:
so, where is the msitake i had? how can i do to run the app form sbl_ospi ?
HI Joe,
Which MCU+SDK version is this?
but, if I check the box [Disable Auth For Application Image], there is also a status that the app cann't run:
From the logs it seems after you disable the authentication for the app image, the SBL is able to load the application, I don't see any failure logs. Which application image you are trying to boot here?
Best Regards,
Meet.
sdk: ind_comms_sdk_am243x_09_02_00_15
flash: IS25WX064
chip: AM2432
i have test teh examples of ospi_flash_diag/dma/io, and all of these can be run correctly.
Hi Joe,
i have test teh examples of ospi_flash_diag/dma/io, and all of these can be run correctly.
Could you please confirm if your original issue with the booting is resolved, as you mentioned you can run this example correctly now?
Best Regards,
Meet.
Hi Meet,
first, the examples of ospi_flash_diag/dma/io can be run correctly with the sdk_mcu in ind_comms_sdk_am243x_09_02_00_15 using the flash chip of IS25WX064.
then, when using the sbl_ospi th boot app, the app can not run, the uart debug information are:
but, when i change the flash chip to S28HS512T(both change in syscfg and board),the sbl_ospi can run the app correctly.
so ,the problem is also why i cann't using the is25wx064 in sbl_ospi to runing the app? where are the problems?
Best Regards,
Joe.