This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Comparing clocks in different RM4 uC

Hi,

In our application we're intended to have two RM4 which use identical 16MHz oscillators. Reading the spnu503 I found some information about DCC and ECLK.

I would like to set ECLK of uC1 to retransmit the signal of its oscillator. This would be connected to TCK in uC2 as source for DCC2. In the other way around, oscillator of uC2 as source for DCC2 in uC1.

As in spnu503, it can be done by setting CNT0 CLKSRC = 1010 in DCC2 and SEL_ECP_PIN field in clock test register as 0000. Is that true?

Many thanks in advance.

  • Hello Francisco,

    I will ask one of our engineers to respond to you soon.

  • Francisco,

    You will have to use the EXTCLKIN1 and EXTCLKIN2 of counter 1 on the DCC1 module for this task. All other inputs to DCC1/2 modules are internal signals. You can use the following code example for generate the ECLK with difference sources and setting up DCC1 with OSCIN as reference on counter 0 to make the period on input to counter 1.

    void ECLK_Config(unsigned int mode, unsigned int clk_source) // mode =0 normal, 1 test; clk_source =0 oscin, 1 pll
    {
        register SYSTEM_ST *ptr  = (SYSTEM_ST *)SYSTEM;
        ptr->SYSPC1_UN.SYSPC1_UL = 1;  // Functional ECLK pin
        ptr->ECPCNTLR_UN.ECPCNTLR_ST.ECPCOS_B1 = 1; // Eclk Continue on Suspend

        if (mode == 0)  //normal ECLK mode
        {
            ptr->ECPCNTLR_UN.ECPCNTLR_ST.ECPDIV_UB = 1;   //ECLK = VCLK/2
            if (clk_source == 0)
                ptr->ECPCNTLR_UN.ECPCNTLR_ST.ECPSSEL_B1 = 0; //0 for VCLK
            else
                ptr->ECPCNTLR_UN.ECPCNTLR_ST.ECPSSEL_B1 = 1; //1 for OSCIN
        }
        else  //Clock Test Mode
        {
            ptr->CLKTEST_UN.CLKTEST_ST.CLK_TEST_EN_B4 = 5;
            ptr->CLKTEST_UN.CLKTEST_ST.SEL_ECP_PIN_B4 = clk_source;
        }
    }

    unsigned int DCC_Cycles(unsigned int CLK_Source,unsigned int Test_Time)
    {
        register unsigned int Cycles;
        register DCC_ST    *DCC_Ptr = (DCC_ST *) DCC1;

            /* Set up the DCC module */

            /* Clear any flags set in the DCCSTAT register */
            DCC_Ptr->DCCSTAT_UN.DCCSTAT_UL = 0x3;

            /* Counter 0 will be loaded with test time (count) */
            DCC_Ptr->DCCCNTSEED0_UN.DCCCNTSEED0_UL = Test_Time - 4;
            DCC_Ptr->DCCVALIDSEED0_UN.DCCVALIDSEED0_UL = 4;

            /* Set up Counter 1 for max time */
            DCC_Ptr->DCCCNTSEED1_UN.DCCCNTSEED1_UL = 0x000fffff;
            
            /* Enable selected clock as source for counter 1 */
            DCC_Ptr->DCCCLKSRC1_UN.DCCCLKSSRC1_UL = 0xA000|CLK_Source;

            
            /* Start count, enable single shot, done and error flags */
            DCC_Ptr->DCCGCTRL_UN.DCCGCTRL_UL = 0xAAAA;

            /* Wait until the DCC Done and/or ERROR flag is set */
            while (!(DCC_Ptr->DCCSTAT_UN.DCCSTAT_UL & 0x3));

            Cycles = 0xfffff -  DCC_Ptr->DCCCNT1_UN.DCCCNT1_UL;

            return Cycles;
    }

    Thanks and regards,

    Zhaohong

  • When applying Zhaohong's advice, please remember to utilize a clock divider on the ECLK output signal which allows the internal frequency to be adapted suitable for input on the EXTCLKIN pins.  Reducing the frequency will also help mitigate potential EMI issues of driving a high speed clock between the devices.

    Regards,

    Karl

  • Thanks you all, we will try to follow those recommendations.